This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24075: SYSOFF to turn disconnected BAT to VOUT (don' have DC input in Vin pin)

Part Number: BQ24075


HI 

I saw about 2V at the OUT when OUT pin is floating (SYSOFF is high, Battery is attached). When 1 mA loading is applied, the voltage at OUT is dropped to 0V.

What happened? 

How do I make OUT pin is 0V without Battery energy loss? (I don't want to loss Battery energy.)

Thanks.