Other Parts Discussed in Thread: UCD3138
I have a new application where we need 15V output with max 8.5 amp, say 9 amp.
Input is DC coming out of 3ph PFC with 380V well-regulated voltage. Say, 5% tolerance on it. So input min is 360 V and max is 400V.
We are using the SLUC644 spreadsheet to calculate estimated values of various R, C, L etc in the circuit. We have already run the calculations for a 12V@4 amp, got all values. We are about to go for the fab even. Switches are selected from TIDA01622 design guide in addition to the UCC28780 d/s and our discussions on this forum.
But in 15v case, we get #VALUE in Rcs row.
Cannot determine why is that & which inputs are causing this to happen. They are basically the same as for the 12V case.
I have reported earlier that another value always comes up as -xxx : that is Ropp. Never could determine what causes that.
Any help in fixing Rcs values will be greatly appreciated. So goes for Ropp.
-r