This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62177: effects of other power src on input/outpout when TPS62177 is un-powered?

Part Number: TPS62177

Team,

The use case is:

TPS62177 is powered off as there are no VIN source.
However an other power source provide 3.3V to the TPS62177 SW and VOS pins (see pink arrow on picture below).
I assume that the SW output and VOS input are not fail-safe pins.

-What would be the effect on input and output pins? and are the effect the same on both input/output?
-Does it affect the long term reliability?
-What do you advise in such case  (how to protect INPUT/OUTPUT pins, acceptable period of time that INPUT/OUTPUT pins can see a voltage,..etc)?
-Any existing TI reference design that shows protection for this use case?

Thanks in advance,

A.