Hi team,
I have a question about the transition speed of Vout.
Why does it take as much as a second to reduce the output voltage if I dynamically change the feedback voltage divider resistance with "Vout Select"?
When the output voltage is raised dynamically with "Vout Select", it switches within 1 ms, but when the output voltage is lowered dynamically, it switches in about 0.1 to 1 second.
For example;
When I pulled out the jumper connector attached to 3.3V selection by "Vout select", Vout became 15V within 1ms.
However, when the jumper connector was attached to the 3.3V selection position, it took 1.3 seconds for the output voltage to drop to 3.3V.