I'm using the BUF16821A and only using OUT1 through OUT10, is it ok to leave OUT11 through OUT16 and Vcom2 unconnected? Currently OUT11 through OUT16 and Vcom2 are programmed for 0V, is this OK?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I'm using the BUF16821A and only using OUT1 through OUT10, is it ok to leave OUT11 through OUT16 and Vcom2 unconnected? Currently OUT11 through OUT16 and Vcom2 are programmed for 0V, is this OK?
Hello Robert,
It should be ok to leave the un-used OUTx/VCOMx un-connected, especially since they are programmed for 0V.
Kind Regards,
Liaqat