This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/UCC2895-Q1: Output max current

Part Number: UCC2895-Q1
Other Parts Discussed in Thread: UCC28950-Q1, TINA-TI, UCC28950, UCC28951-Q1

Tool/software: WEBENCH® Design Tools

Hi team

My customers want to simulate UCC28950-Q1 with the WEBENCH.

  • Input condition: 800V
  • Output condition: 24V / 10kW

The WEBENCH screen shows the maximum current of 300A as shown below.

Is current above 300A impossible to review with UCC28950-Q1?

We ran simulation to 250A condition on the WEBENCH.

The following message will be displayed and the simulation will not work.

Is there a way to make this possible?

We are going to review constants for the compensation circuit value with the WEBENCH.

Can I get Bode plot simulation results when the simulation runs normally?

https://webench.ti.com/appinfo/webench/scripts/SDP.cgi?ID=F4190581442DED59