Other Parts Discussed in Thread: UCC28950-Q1, TINA-TI, UCC28950, UCC28951-Q1
Tool/software: WEBENCH® Design Tools
Hi team
My customers want to simulate UCC28950-Q1 with the WEBENCH.
- Input condition: 800V
- Output condition: 24V / 10kW
The WEBENCH screen shows the maximum current of 300A as shown below.
Is current above 300A impossible to review with UCC28950-Q1?
We ran simulation to 250A condition on the WEBENCH.
The following message will be displayed and the simulation will not work.
Is there a way to make this possible?
We are going to review constants for the compensation circuit value with the WEBENCH.
Can I get Bode plot simulation results when the simulation runs normally?
https://webench.ti.com/appinfo/webench/scripts/SDP.cgi?ID=F4190581442DED59