This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM7800: LM7812

Part Number: LM7800

Hello TI,

Test setup:

We are using the following TI components on our PCB: LM7812 and LM7912

The LM7812 provides +12V and LM7912 for -12V which are supplied by +15V / -15V.

!! With respect to the used electrical circuit the output of the LM7912 (-15V) is connected to the output of the LM7812 (+12V) by using a diode.

The anode of the diode is connected to -12V. The cathode is connected to +12V.

Test procedure:
Step 1: Switch on -15V input voltage first.
Step 2: Switch on +15V input voltage.

Test result:
Unfortunately our test engineer found out that the +12V power supply drops to 0,8V.


If the diode is removed from the voltage regulators the power supply is stable.
If the test procedure is inverted the +12V power supply is stable, too.

QUESTION TO ST:
Can you explain this behavior ?
Why does the output voltage of the LM7812 depends on the power on sequence ?
Is there any protection mechanism of the device which is responsible for this behavior ?

Thank you !