Hi Sir
Does LM27313 + DAC can be use in Dynamically Adjustable Output(Vin 5V/Vout 12V~20V Iout 0.1A)?
If yes, may you pls help check attached circuit is ok or not?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Sir
Does LM27313 + DAC can be use in Dynamically Adjustable Output(Vin 5V/Vout 12V~20V Iout 0.1A)?
If yes, may you pls help check attached circuit is ok or not?
Hi Boge,
Please add a 10uF input capacitor.
Is net FB connected to FB_10V though a 1k ohm resistor? Please change it to a 10kohm resistor.