This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP87562-Q1: Control of Enable pins during configuration

Part Number: LP87562-Q1

The configuration guide(SNVU590) states,

It is recommended that the ENx pins be driven low to until the device is configured to the desired settings.

Can the driving of the Enable pins during configuration be accomplished with register writes via the I2C bus?

I'm using 3 LP8756x-Q1 devices and the mcu used for programming is on another board. I prefer to not have to hard wire these pins and  route 12 enable signals(4 per PMIC) to the daughter card.