Hi Team,
Please help me answer the follow question, thank you so much.
The typical value at the time of Battery FET turned off of VSYS(REG) is described in datesheet, but when the FET is off, does min (VBATREG + 1.5%) means min 3.5 V +1.5%?
Could you tell me the difference between VSYS(REG) and VMINSYS?
Is VSYS(REG) the typical value when the Isys max is 3A on the load of SYS side?
The SYS side is also branched to battery charge and discharge, but is Isys max 3A the sum of SYS side load and battery?
Could you tell me the relationship (distribution?) of the current charge/discharge between the load on the SYS side and the battery?
Best Regards,
Tom.Liu