This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS55165Q1-EVM: TPS55165Q1-EVM Schematic question

Part Number: TPS55165Q1-EVM
Other Parts Discussed in Thread: TPS55160Q1-EVM

Hello TI;

 We have some TPS55165Q1-EVM, and we need to use this regulator as buck-boost to generate 5V (300mA) based on an input Voltage range from 3.5V to 9V.

We are using the User's Guide (SLVUAY1–November 2017).

There is a "Figure 3. Schematic Diagram—No Variations

And there is also "Figure 5. TPS55165Q1-EVM Schematic Diagram—Assembly Option".

1-Which one should we use as reference for the actual EVM?

2-Which one should we use as based to based our schematic for the requirements described above.

3-Why is there a difference between these 2 schematics?

3a- Why are the diodes and other components of Figure 3 removed in Figure 5?

3b- Not having these devices , could cause a mal function or performance degradation of the regulator?

Regards;

Thanks