Other Parts Discussed in Thread: LMZM23601
Hello TI;
We will use the LMZM23600V3SILT or te LMZM23601V3SILT, to genereta a 3.3V Voltage Rail.
These are our main requirements:
- The Power Supply PWA shall provide a 3.3VDC +10%/-5% voltage rail with an operating range of 0mA to 200mA continuous current.
- The 3.3VDC voltage rail shall not have a voltage dip of more than 20% with an instantaneous output current of 600mA for 100uSec.
Since we will be working under 200mA, we want to use the 500mA version (LMZM23600V3SILT).
The questions is can the LMZM23600V3SILT accomplish requirement number 2 above?
Regards;
Luis