Hi,
I've designed a PCB using LM5119Q. The circuit is designed to generate 27V, 1.6A and 38V, 4.3A. The circuit is operating properly under no load conditions. If the load is connected after the required voltages generated, the circuit is able to source the required amount of current. But if the circuit is switched on with the load connected beforehand, the circuit is not able to source the required amount of current and the output voltages do not reach the required levels. Please find attached the schematic for your reference.
Please help me with this.
Thanks and Regards,
Karthik