The TPS798 datasheet says:
Maximum ratings:
EN -65v to 60v
EN to IN differential 0.6v to VIN
I'm not sure I understand the differential rating of 0.6v.
If I tie EN (which enables the regulator) to IN I have a differential of zero.
Can you clarify the restrictions on the EN to IN differential? Is it along
the lines of:
EN to IN differential -IN to 0.6v
meaning that EN can be at ground (aka IN more negative than IN) and
up to a maximum of 0.6v more positive than IN.
Specifically I'm looking to confirm whether EN is allowed to be more
positive than IN or if a voltage translator is required.