Hi Experts:
My customer is using the UCC2813-2 for the power design , the turn on threshold is 12.5V, however, the maximum rating of VCC is 12V , so I have two questions:
1) The start up voltage should be above the 12.5V which will beyond the maximum rating ,is it risk to damage the device.
2) If the device has started up , should be also need to supply the voltage (if supplied from the output) which will above the 12.5V?