This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TL750M: TL750M12CKVURG3

Part Number: TL750M

Could you please provide recommended effective input and Output capacitance value for TL750M12CKVURG3?
Currently I will use  > 10uF electrolytic capacitor at input and output .

  • Hi Ashish,

    The TL750M datasheet recommends minimum of 0.1 uF input capacitor and 10 uF output capacitor. For the 10 uF output capacitor, up to 2 ohms ESR is required. A resistor in series with the output capacitor can be used to meet the required ESR. For details, see page 6 of the datasheet.