Other Parts Discussed in Thread: UCC28600, UCC28710, UCC28051, TPS92210
Hi
I have an AC/DC solution in evaluating TI
The spec information are as follows, can provide suggestions?
I have seen the LM5023.
http://www.ti.com/tool/PMP7883
and also
http://www.ti.com/tool/PMP8655, is this solution to change the transformer? if change the transformer can give me transformer parameter information?
and I also study UCC28600, UCC28710
VIN: 90-300VAC
VOUT: 24V / 2.5A
PF> 0.8
THD <30%~15% (depending on load)
PCB size can't too big