Dear Team,
Can you double-check the schematic is there any concern here?
BR
Kevin
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Team,
Can you double-check the schematic is there any concern here?
BR
Kevin
Hi Kevin,
I will look into the schematic and get back tomorrow.
Meanwhile if you could share the operating current and voltage requirements, that will enable better review feedback.
Regards,
Kari.
Hi Kevin,
Schematic comments:
MOSFET selection, rating and RdsON are good.
RSET resistor can be changed from 59K to 76K, this will reduce the limit for reverse current and cause little momentary dip during switchover.
With 59K, reverse threshold is -4.28mV, reverse current is -1.66A, with 76K it will be close to -3mV and -1A.
Transient protection:
Absolute maximum rating of this device is 18V and I don’t see any TVS or protection at the input.
Customer may be aware , but needs care here.
Regards,
Kari.