Hello team,
Customer is needing to drive a single 1A (3W) LED with 2.5-3V working voltage and considering TPS92512HV for constant current source and PWM dimming. Would we have any other recommendation besides 512? I think 513 could work if current is set to 1A and not higher. Vin is at 24V.
Another question that comes to mind, how are we setting Vout min and max bounds? For example how are the limits set in the EVM design? Is it just based on application? Reason to ask is to make sure 2.5V Vout can be supported with the right design.
Section 8.4.2 of datasheet discusses the Ton(min) limitation, but is there any other point to consider? Assuming equation 12 in datasheet and assuming 24V input and switching frequency 100kHz, then can we say Vout(min) = 24V*100kHz*140ns = 0.336V ?
Thanks!
*Post has been updated to reflect Vin info from customer.