Hi Support, please review attached.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Ikon,
What is the ESR of the output capacitors?
Hi John,
Input: C282 is 22uF, T498C226M016ATE400, ESR=400mohm
Output: C286, C287 is 220uF, T591D227M010ATE080, ESR=80mohm
Thanks.
Ikon,
That design is right on the edge for stability. One additional 220 uF at the output would be better. You will need some ceramic bypass capacitor on the input. 10 uF is recommended. The BOOT capacitor is a little large. it should be between .022 uF and 0.1 uF, 0.047 uF is recommended.