Other Parts Discussed in Thread: LM5155
Hi ,
Could you please confirm that I fill is correct?
Warm Regards,
LinLM5155_Excel_Quickstart_Calculator_for_Boost_Converter_Design.xlsx
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Lin,
Thank you for considering the LM5155. Your inputs are basically okay but there are a few problem:
1. Your min Vin is 11V. Why set the UVLO threshold at 3V?
2. For 210V output, 100mV ripple voltage is a very tough spec. Most designs usually has 1% ripple voltage, i.e. 2.1V in your case.
3. The entire design may not work well. Note that you need 95% duty cycle to achieve output regulation. However, the datasheet EC-table specifies the max duty cycle may drop to 80%.
For 11V to 200V step up ratio, we usually recommend a DCM (which is not supported by this calculator), and also two stage circuit, with the main boost plus a charge pump. Please refer to the following ref design. The IC is different but the concept is the same. We are planning to releasing a LM5155 ref design for similar application, but it may take some time to show on the website.
http://www.ti.com/tool/PMP20183
If you need close design support, please contact TI sales personnel or a FAE in your region.
Thanks,
Youhao Xi, Applications Engineering.