This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Could you let me know the package information as follows?
P/N:
5962-8670410VPA
・Package material/ base plating /plating (ex. Ceramic(Alumina)/Ni/Au
・Lid material/ base plating /plating (ex. Covar/Ni/Au
・Package cavity wall thickness(mm) (ex. 0.25mm
・Lid thickness(mm) (ex. 0.25mm
・Part weight(typ. grams) (ex. 3.5g
・Part weight(max. grams) (ex. 4.0g
We'd like to use it for a thermal & radiation analysis.
Regards,
Tom8883.cavity wall and lid definition.pdf
Hey Tom,
I will get this information as soon as possible for you and respond back.
Thanks,
Daniel
Hey Tom,
We are still working on getting this information.
Thanks,
Daniel
Hey Tom,
Package material/ base plating /plating : Glass Frit
・Lid material/ base plating /plating: Glass Frit
・Package cavity wall thickness(mm) 2.54,3.048 ( x, y dimensions)
・Lid thickness(mm) 0.787
・Part weight(typ. grams) 1
Sorry for the delay.
Thanks,
Daniel