This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Team
My customer is using UC2843 as Buck. The input voltage from 350-800V, output voltage is 300V. The power is 500w.
1)They have some issue about the output wave. The device is powered by 15V and the input can't connected. UC2843 refference output normal. But the driver output is abnormal. Attached are the scope wave. Not all device abnormal.
2) the work well devices, when the duty cycle rise, the output will oscillate harmonically. Could you give some comment about it? How to adjust the compensation network?
Hi Xiao Zhu,
1) It seems not caused by unstable loop.
May you attach the schematic here or email at teng-feng@ti.com
2) This is a paper which provides provides peak current mode buck converter loop modeling. It is better to adjust compensation loop by using a loop analyzer.
http://www.ti.com/lit/an/slvae09a/slvae09a.pdf
Regards,
Teng