Hi,
I am using LMR14050SEVM and noticed that evaluation board is specked at 7V input minimum but IC is capable of up to 4V input. When I apply 7V input with a 4A load at 5V, output starts cycling from 0V to 5V. and Inductor becomes noisy.
Is IC not capable to handle 7V input?
Why IC and Eval board specked differently?
If not, what could be the reason for the eval board not working reliably at 7V input with 4A,5V output?