This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMZM33603: About Inverting circuit

Part Number: LMZM33603
Other Parts Discussed in Thread: LMZ14203H, LMZ14203, LMZ34002

Hi,

Customer wants to use LMZM33603 under the following conditions:
・Vin=24V (AC adapter 24V±10%)
・Vout=-12V
・Iout≒0.5A

I have two questions.
1.Customers want to use ACadapter with 10% accuracy.
  Therefore, customers want to allow an input voltage of 26.4V.
  Is this usage condition acceptable?
  And Is it acceptable depending on the load current?
       
       

2.About Switching Frequency vs Output Voltage 
  Customers want a table of Inverting circuit versions.
  Can you provide that information?

       

Best Regards,
Yusuke