This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24715: What is the correspondence between the Vout and Vin of the BQ24715 in different Cell settings?

Part Number: BQ24715
Other Parts Discussed in Thread: BQ24157

Hi Sir 

The measure waveform, may we check as below questions with you?

The questions as below:

  1. What is the correspondence between the Vout and Vin of the BQ24715 in different Cell settings?

        2. Suppose that in the case of 3Cell, if each Cell is fully charged at 4.2V, does Vin need a higher value than the output (Ex: 12.6V)?? How much voltage does Vin need to output higher than?

How much voltage should I add if needed? Is there a relationship??

                                                                            Bogey

BQ24175.docx