Hi
At page 22, it is mentioned as below.
. Ferrite based inductors are preferred to minimize core losses when operating with the frequencies used by the LM26420.
This means the inductor is recommended the ferrite type.
Is the metal core type possible to use ?
I understand the metal core is small inductor value but it can be used for large current application. And it has high core losses. (Rac?)
Is there any other concerns if we use the metal core type?
Best Regards,
Koji Hamamoto