This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24266: External NTC Monitoring Review Request

Part Number: BQ24266

Hello,

Could you please review my customer design? He says CHG does not disable when Vhot<1.4V (Vdrv * 0.3).

He connects LED to /CHG pin to check that.

<Parts used>

THermistor

0℃:Rcold=27.22kΩ/60℃:Rhot=3.01 kΩ

<Designed value>

RLO:13kΩ / RHI:5.9 kΩ

<Test procedure>

Heating thermistor with a hair dryer, and then observe the TS pin.

Heat until TS pin voltage goes below Vhot = 1.4V.

When charging stopped, /CHG LED is supposed to turn off.

Please feel free to correct me if I'm wrong. Thank you.

Regards,

Itoh