This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61071: CparR1

Guru 16770 points
Part Number: TPS61071

Hi

Let me confirm the position of CparR1.

The customer uses R1=820K and R2=91K to get 5V output.

So CparR1 will be needed.  Is it correct that the placement of CparR1 like below figure?

BestRegards