This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54386: dual channel with positive and negative outputs

Part Number: TPS54386

Hi team,

My customer is looking for a +10V 3A & -8V 3A dual channel power supply for OLED screen. I'm wondering is it possible to make it happen with dual channel buck like TPS54386. I've do tests on TPS54386 EVM and it's capable of providing 2A for each channel at the same time. Simplified schematics is illustrated as follow. Basically 2 channels with 18V & 8V outputs, using 8V as ground.

The one disadvantages I've think of is that +10V is easily affected when short or open circuit happens at -8V since it's the difference of 2 channels. Any other comments on this configuration? Has anyone actually do this in practical? 

Thanks so much.

Best Regards,

Charles Zhao