Team,
Could you make sure whether my calculate is correct or not in below conditions.
Must:
- Vs=6V to 36V
- Vz=5V
- Iout>50mA
Accuracy >0.5%
My calculation is as below
Iz is chosen from datasheet spec of the minimum cathode current.
Is it okay to use the Rs value even the Vs should be changed from 6V to 36V?
If yes, how do I realize the above condition?
Thanks,
Uchihara