Other Parts Discussed in Thread: TPS62160
Hi
I have a question about Vfb of TLV62585.
Vfb is defined 588mV(min), 600mV(typ) and 612mV(max) at PWM mode, 2.5 V ≤ VIN ≤ 5.5 V, -40°C to 125°C in 6.5 Electrical Characteristics.
If this device operate low drop, may I understand that Vfb is same value above stated?
Or will it be out of conditions at low drop operation like TPS62160?