Hi Team,
My customer is using LM20343 for 24Vin_15Vout/2.5A application and they would like to check some parameters in datasheet:
- Max Duty Cycle: datasheet shows typical value is 80%, but didn’t shows the Min value, could you help to provide this data?
- Feedback resistor suggested only up to 5V, and my customer is using it in 15Vout application, I’m wondering if you can comments what value should we choose.
- I didn't see Absolute Maximum Ratings has temperature range like -40-150C, could you help to confirm maximum temperature range for LM20343?
thanks.