This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2561A-Q1: Higher Voltage Replacement

Part Number: TPS2561A-Q1
Other Parts Discussed in Thread: TPS2513, TPS2561

I have been working with the TPS2513 and TPS2561 for wiring a USB port. However, I am having some trouble getting the output voltage that I want while staying within the 7V maximum voltage constraint for the TPS2513 and TPS2561. Does TI offer any other chips that have functionality similar to, or the same as, the TPS2513 and TPS2561 but with a higher maximum input voltage? If so, what are the part numbers for these chips?

Thank you.