Other Parts Discussed in Thread: TPS61070,
Hi
I am using a TLV61225DCKR DC-DC in a 3V battery powered application to generate 3V3 from the battery until the battery gets to around 1.7V
The EN pin (Pin 6) is connected to the GPIO pin of a ST microcontroller running from the 3V battery and also has a 10K pulldown to GROUND.
The aim is to use the microcontroller to switch the DC-DC on and off as needed.
When the GPIO is not connected to the EN pin (track cut) and only the 10K is connected to GND the output of the TLV61225DCKR is not 0V but at 2.713V.
If the 10K is removed the output stays at 2.713V.
I cannot get the output of the DC-DC IC to go to 0V.
I have not tried shorting the EN pin to GROUND and will do that now.
Any ideas?
BJ