This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: WEBENCH® Design Tools
Hi,
I want to use the LM5146-Q1 in my power module.
The input voltage range is 35V~60V, and I need a OVLO design at the voltage of >65V,
can you help me how to do the OVLO design with LM5146?
Thanks gavin,
Do you have any typical reference circuit to suggest?
And I also need the output over voltage protection design,when the output >15.5V (Vout=13.8V typical), do you have any solutions ?
Hi ,
Sorry, we don't have typical reference circuit from my side. You can check whether there is any reference or paper.
Gavin