TPS61099EVM-023 or TPS610995 are not working as per the specification given in the datasheet. After reading this document www.ti.com/.../tiduee2.pdf, I decided to use TPS610995 in the design. So designed board using TPS610995DRVR IC. Found the output voltage is ~3.8V whereas the product has a fixed output voltage of 3.6V. To cross verify if it is design related issue, I had purchase EVM also. Even the EVM output is 3.8V. This is a serious issue. Request to please help resolving the issue at the earliest.