Hi Expert,
Is there maximum soft start time spec limitation for TPS54428?
Thanks.
Allan
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Allen,
There is no maximum soft start specification.
Thanks,
jenson
Hi Jenson:
Now i use SS cap 680pF , it can not out 3V3 just about 1V3,when i change the SS cap from 680pF to 8200pF
it can work 3V3 ,so the design have issue ,please help to check it!
Hi Allen,
I don't see any reason why you do not get the correct Vout at 3.3V.
Besides changing CPC24 to 8200pF, can you also try to remove CPC25 then see if you can get the correct output?
On WEBENCH, there is suggestion for minimum soft time to be 1.15ms.
Regards,
jenson
Hi Jenson:
Yes when i remove the CPC25 ,the output is OK.
So what the reason?
Jamie
Hi Jamie,
Did you mean that removal of CPC25 does not fix the issue?
In this case, you need to increase the size of CPC24 because the soft time is probably too short
According to section 7.4.1, CPC24 > Tss(ms) x 6 / 0.765 / 1.1 = 7130pF
regards,
Jenson