Other Parts Discussed in Thread: TPS61099, TPS630242, CC1310, TPS63802, TPS63060, TPS63805, TPS63806, TPS63020, TPS63036
Hi,
1. I have an application where I need to supply(controller) 3.3V and min is 3V and using LiMnO2 CR2477 Coin Battery which rated 3.3V,1000mAh.
My load may take max of 200mA but in the Data sheet they have clearly mentioned that Supply shout be able to provide max of 1A.
have checked these two TPS61291 OR TPS61099 as both are boost latter without bypass mode. But unfortunately I'll not be able to use both of these are rated for 200/250mA.
Do you recommend any other part number with max load current above or equal to 1A with bypass / Buck-boost.
2. We might change the battery to other Li Ion (may be cobalt) which full charged will have 4.2V and has to maintain 3.3V So in this case Boost with bypass won't be helpful. Is the Buck-Boost is the only way to achieve this?
As I'm looking into this TPS630242 which has a lot less efficiency at 50-55% at less current which in our standby current (100uA). Any suggestions?
Looking forward to your answer.
Thanks.
Lakshminarayana K N.