Other Parts Discussed in Thread: TPS54560
I see that there was a previous question about the difference between the Q1 and non-Q1 versions of the part. Your answer was something to the effect of "no difference in functionality, but more testing for -Q1".
However, I notice on the datasheets for the two parts a difference in section 7.3.7, regarding the EN pin. On the -Q1 data sheet, it says that there is an internal 5.8V zener diode to clamp the pin. On the other data sheet it explicitly says that the user should add an external zener diode to clamp EN if the voltage might rise too high. Is this an actual difference between the two versions, or an error in one of the datasheets?
I ask because I am redesigning a board that has used the TPS54560 (older version, no "B"). The datasheets for it and for its -Q1 version both mention the internal zener. I do not necessarily need the extra testing of the -Q1 part, but the extra cost might be worth it to avoid having to add an external zener diode. And regardless, I do not want to make a mistake with the redesign. Other than the zener, it appears that the "B" part is a drop-in replacement.
Please advise.
Thanks,
Rod Hinman