Dears :
customer fund BQ24092 can't shutdown in negative temperature , they need the charger can work in 0-45C, Could you please help check below schematic and give suggestions ? Thanks .
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dears :
customer fund BQ24092 can't shutdown in negative temperature , they need the charger can work in 0-45C, Could you please help check below schematic and give suggestions ? Thanks .
Hello
The TS pin should be connected to an NTC resistor in the battery pack, this will monitor the temp and set 0C / 45C shutdown points.
What NTC is used? Is an additional resistor network used?
Bill:
customer put 10K NTC in battery pack and 250K NTC to ground , they found it will shutdown in -10℃,they need BQ24092 can shutdown at 0 ℃, Please help check if the set is right .Thanks .
Can you tell us what type of NTC the customer is using? We use the SEMITEC 103AT-2 or Mitsubishi TH05-3H103F for our calculations.
Thank you for that information, this ntc meets the same B value that we expect. You didn't include the information for the 250K NTC though. In the standard profile you would have a 0C - 60C operation but you are saying the customer is seeing a -10C - 45 C operation correct? Can you share what 250K NTC they are using?