Other Parts Discussed in Thread: LM5009,
Hi support team.
Please let me know how the output voltage behaves when the current limit occurred.
Regards,
Dice-K
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Dice:
LM5009 Datasheet in 7.3.6 decirpted that Toff will extend when curent hit 0.31A over current threshold. Ton will keep same, so the output will decrease when Toff increased. LM5009A will keep working, but due to Vo derceased, so the total output power will be decreased as well as input current.
Thanks
Daniel li
Hi Daniel,
Thank you for your reply.
Does Vout become 0V?
Best regards,
Dice-K
Hi Dice:
Vo will not drop to 0. Its voltage will depend on the load resistor, Ipeak will be limite to 0.31A, asuming ripple current is 60mA peak to peak, the output current will be limit at 0.28A, Vo~=0.28A*Rload, then FB voltage will decide the Toff time.
Thanks
Daniel Li