art Number: TPS92691-Q1
Tool/software: WEBENCH® Design Tools
HI i am creating a circuit to power a cree xhp 70 @ 2.4a and have used webench to produce the schematic.
However there are 2 open points on the schematic labelled 1 and 2.
1. From reading the data sheet Iadj should be connected to Vcc through a 100ohm resistor, creating a reference voltage. Another resistor can then be positions between Iadj and ground to create a voltage divider and act as anologue dimming.
Is this correct?
2. So far i assume that these 2 open points should be connect to create a path between Csn and Led+. The data sheet examples show conflicting information so i thought i'd ask just to be safe.
Is this correct?