Hello experts,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello experts,
Hi Ryo,
The maximum current is about 34mA for each channel.
Regards
Sean
Hello Sean,
Hi Ryo,
Please refer to the datasheet for 35mA for the maximum current.
Regards
Sean
Hello Sean,
Hi Ryo,
No, for boost topology, when internal switch turns on, inductor install energy, and when it turns off, it not only output current to IFBx channels, but also charge the output capacitors. And since there are two channels for those devices, so the average current of the inductor depends on the detail application.
Regards
Sean
Hello Sean,
Hi Ryo,
You can find this on data sheet spec table, the KISET=920(typical).
Regards
Sean
Hello Sean,
Hi Ryo,
Yes, the maximum current is a system level question, here is an application note that can help you to estimate the maximum current based on the detail application specs.
http://www.ti.com/lit/an/slvaeg0/slvaeg0.pdf
Regards
Sean
Hello Sean,