Hi TI support
We have a question about the suitable solution for super cap charger
- Capacity: 100F
- Voltage: 5
- Charge current: 1A
Could expert give some recommendations in this case
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Paul,
For standalone supercap charger, we recommend BQ24640.
Regards,
Jeff
Hi Jeff F
BQ24640 is use external FET
we found have BQ24130 use internal FET.
with this part, can we input 5V and charge for super cap 4.2 V ?
Please advise,
Paul,
Yes, however, like all of our chargers, the BQ24130 reduces current significantly when the battery is below VBATSHRT=2V. Charge will be very slow when the capacitor is 0V to 2V.
Regards,
Jeff