Other Parts Discussed in Thread: TPS5430, LMR23625,
Please find attached simulation showing an implementation of a Zeta Buck/Boost Converter having 10V < Vin < 13V, Vout = 10V, Iout ~= 1A.
The simulation is based on the TPS5430 (and it's TINA Reference Design) because it has a TINA model that may be used in the inverting buck/boost configuration. This simulation runs quickly, in about 30 seconds.
D1/C3 are the inverting buck/boost components, and C5/D2 are the Zeta specific rectifier and power transfer capacitor to make it operate as a non-inverting buck/boost. I have not optimized any of the values, just threw this together to verify it would basically work.
I would like to use the LMR23625 or LMR23630 in this topology. As I am unable to simulate the LMR236xx devices in the Zeta topology due to limitations with its model, I am asking here if you see any problems operating it in this manner?
Thanks, Best, Steve