This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25601: Power On Reset

Part Number: BQ25601

Hello

My customer chosen BQ25601 for their new project, and they has  started evalluating

their PCB.

Q1 POR time

When VBUS rises above VVBUS_UVLOZ or BAT rises above VBAT_UVLOZ ,

how much time is necessary between "VBUS rise above VVBUS_UVLP" ,

and "I2C interface is ready for communicaiton " ?


My customer says approx 300ms  ? wait time for i2c communication

should be necessary after Power on in their PCB.

But I don't know whether it is correct or not.

Furthermore, we don't know  wheter it varies depend on VBUS slew rate or temperature or any other condition ... Or,  it doesn not vary ( POR time is stable).

Would you please advise above?


Q2 I2C state under POR

Customer says SCL=High during POR, but is it correct?


Q3 INT pin

How can customer detect POR- finish?  Using INT pin?


I had attached customer's schematic.

According to customer , Icc of MCU is small( 1~2 mA) and sink current from REGN LDO shoould be

negiligible.

Thank you for your support.

Best Regards

Best Regards

  • Hi,

    1. ""VBUS rise above VVBUS_UVLP" time depends on VBUS rising slew rate which is not controlled by the charger.

    2. It depends on if the host tries to write or read the charger registers.

    3. It is better to read the charger status via I2C.

    4. Please double-check your schematic with the application example on the d/s and the BQ25601 EVM.

    Thanks,

    Ning.

  • Dear Ning-san

    Thank you for your comment. Please close this.

    Thank you again