Other Parts Discussed in Thread: CSD23202W10
I am designing a bq25505 into a wind harvesting device. The kinetic energy harvesting is done by a turbine connected to a small brushed DC motor used as a generator.
Three issues:
1. The generator output impedance is around 70 ohms. Are there specific input issues I should address when using this fairly low impedance source as an input to the bq25505?
2. The generator output has the potential to exceed the 5.1V input limit to the bq25505. I plan to clamp the bq25505 input to around 5V with a zener diode.
3. What about negative excursions on the input to the bq25505? What kinds of internal protection does the bq25505 have on it's input for negative voltage inputs? I don't expect the input to go negative except in rare situations (turbine reverses, or generator connected backwards) but I want to protect the harvester chip and input cap from those situations. Is there a diode clamp on the bq25505 input to protect from negative input? If so, what is the current limit on that internal diode? I need to determine whether I need to supply an external diode clamp on the bq25505 input to protect from negative excursions. I don't want to use a diode bridge, because it causes to much voltage drop.