This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM25116: Instant current issue

Part Number: LM25116
Other Parts Discussed in Thread: CSD18563Q5A

Hi,

My customer have used LM25116 in  a 24V in 5V10A out design. so far, they are doing test.  recently, they found the boot up of their CPU will cause a extra 10A peak instant current,  added this ,their system will experience a 20A peak  instant current, they are  worried about the temperature rise of the MOS.

so far, they are using CSD18563Q5A for both high side and low side. they found  the low side MOS can't  passed the stress test when they increased the load  current to 16A  for a short time, the temperature of low side MOS increase dramatically.  so far, They don't have good  solution and want us to suggest a MOS which can better deal with this situation.  looking forward to your suggestion. thanks.